Getting this error while trying to use mcu config tools for mimxrt1062.. Please help
Hello, my name is Pavel, and I will be supporting your case, in some cases, the issue is because the example is for the EVK, but the MCU is not the same on the board. I reviewed your image, and it seems you did modify the example for the teensy. I recommend opening a new project with the right MCU and importing the example.
Best regards,
Pavel
I imported a new SDK example but error is still coming, please help.
Hello, could you tell me the full number of your teensy board?
Best regards,
Pavel
Hello Pavel,
Teensy 4.1,
Although I think this problem is not about teensy 4.1. As in the aforementioned screenshot, I have not done any changes in the example. I directly imported the example and tried pin configuration.
Hello, I test on my side with the same example, but I cannot reproduce the issue.
Maybe you could try to change the MCU before opening the Config tool.
Best regards,
Pavel
I did that as you suggested, but still same error.
Then I imported the example for i.MX RT1010, and tried pin configuration on it and still same error.
Means on my system pin configuration is working fine only for the i.MX RT1050.
Then I downloaded the mcu expressor config tools separately and installed that in that 1050 is only present as shown.
Next I downloaded MIMXRT1060-EVKB_ConfigTools_data and tried to import it but this error comes
Hello, sorry I cannot reproduce this issue I recommend downloading again the SDK and the IDE new version. If you are using Win11 there are some reports that the tools do not work as expected use Win10.
Best regards,
Pavel