i.MX RT1051 + mbedTLS + TLS 1.2 + DCP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1051 + mbedTLS + TLS 1.2 + DCP

1,804 Views
mathieu_bordere
Contributor I

Hi,

I'm trying to setup a TLS 1.2 connection with mbedTLS on a i.MX RT1051 with Hardware/DCP accelerated AES128 and SHA256.

For this to work I need to setup the mbedTLS heap allocator to use non-cached memory that can be accessed by the DCP.

When I place the mbedTLS heap in DTCM memory, I'm able to setup a TLS connection and all seems to work fine, however when I move the mbedTLS heap to non-cached SDRAM I fail to setup a TLS connection.

Non-cached SDRAM is setup like this in the MPU

/* Region 9 setting, set last 2MB of SDRAM can't be accessed by cache, local variables which are not expected to be accessed by cache can be put here */
    MPU->RBAR = ARM_MPU_RBAR(9, 0x81E00000U);
    MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_2MB);

Is this the correct setting?

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,669 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mathieu Borderé,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Yes, it's correct.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,669 Views
paolo_chiesa
Contributor I

I have a similar problem: i'm able to run the demo of mbedtls client on imxrt1050 ONLY when disabling cache, but I'm not able to run the same demo with cache enabled because of the DCP/DMA access to cache.

How can I move MBEDTLS on a one not cacheable section? I have already declared a uncacheable section.

0 Kudos
Reply

1,669 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Paolo Chiesa,

To provide the fastest possible support, I'd highly recommend you to refer to the application note:
https://www.nxp.com/docs/en/application-note/AN12042.pdf for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply