howdy!
In the selection tables for i.MX RT, some part-nos are listed with CANFD + FlexCAN vs. some just list FlexCAN. A bit confused here since the NXP datasheet for FlexCAN lists CAN-FD as a supported protocol.
Please help explain the difference between a 'hard' can-fd phy vs the flex-can variant.
解決済! 解決策の投稿を見る。
Hey dav1,
all iMXRT devices which support CAN use the FlexCAN-IP.
The FlexCAN-IP supports CAN 2.0. On some devices the FlexCAN is extended to support also CAN-FD. This is the case for one CAN-Interface on the iMXRT106x Family and all on the iMXRT117x-Family.
I think NXP calls the improved FlexCAN interfaces CAN-FD to distinguish between both. If you use only CAN 2.0 both variants of this interface are identical in use.
Best Regards
Hey dav1,
all iMXRT devices which support CAN use the FlexCAN-IP.
The FlexCAN-IP supports CAN 2.0. On some devices the FlexCAN is extended to support also CAN-FD. This is the case for one CAN-Interface on the iMXRT106x Family and all on the iMXRT117x-Family.
I think NXP calls the improved FlexCAN interfaces CAN-FD to distinguish between both. If you use only CAN 2.0 both variants of this interface are identical in use.
Best Regards
thanks, I was hoping for CAN-FD being possible on any FlexCAN IP block.
but you're right, it's limited to i.mxrt106x +
thanks, I was hoping for CAN-FD being possible on any FlexCAN IP block.
but you're right, it's limited to i.mxrt106x >