i.MX RT cpu family USB OTG dual role

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT cpu family USB OTG dual role

跳至解决方案
1,059 次查看
uwe_strempel
Contributor I

Hi,

can the i.MX RT cpu family (106x/105x/117x etc.) run usb otg dual role (host/device) at same time?

Best regards

Uwe

0 项奖励
回复
1 解答
1,051 次查看
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

在原帖中查看解决方案

2 回复数
1,052 次查看
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

1,036 次查看
uwe_strempel
Contributor I

Hi Mark,

thank you.

That information helps me alot.

Regards

Uwe

0 项奖励
回复