Would the MIMXRT1062CVL5A CPU work @600Mhz ok or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Would the MIMXRT1062CVL5A CPU work @600Mhz ok or not?

893 Views
StephenYeh
Contributor III
Would the MIMXRT1062CVL5A CPU work @600Mhz ok or not?
0 Kudos
Reply
3 Replies

879 Views
StephenYeh
Contributor III

Hi Sir, 

If our customer setting the CPU frequency to 600Mhz, will cause CPU hang issue or not?

 

0 Kudos
Reply

873 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

1) If our customer setting the CPU frequency to 600Mhz, will cause CPU hang issue or not?
-- We'd highly recommend the customer don't do that, as it can't guarantee the MCU can work steadily in a long time with such a high core frequency.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

885 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Would the MIMXRT1062CVL5A CPU work @600Mhz ok or not?
-- No, the maximum core frequency is 500 MHz.

jeremyzhou_0-1626069268425.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply