Looking at this question: How to burn BT_FUSE_SEL on RT1050
there is some code that should enable burning of the BT_FUSE_SEL and FORCE_INTERNAL_BOOT fuses. However, when I try and do the re-calculation for ipg_clk of 150 MHz, I stumpled upon what I think is an error in the original code ?
I have a feeling that the timings above are not correct (or, very likely, I'm misunderstanding the numbers/calculations) ?
From the comments in the code from the link above, they are calculated for ipg_clk of 132 MHz, but if I calculate the resulting timing values using formulas in the Users Manual for 132 MHz also,
I get the following:
// Value at the start of line is [xx] which is number of nS at 132 MHz
// Timing values at 132 MHz:
// int timing = OCOTP_TIMING_STROBE_PROG(1325) | OCOTP_TIMING_RELAX(2) | OCOTP_TIMING_STROBE_READ(11) | OCOTP_TIMING_WAIT(24); // ipg_clk=132MHz, Calculation described at Chapter 22.4.3 OTP Read/Write Timing Parameters
//
//
// [189] WAIT = tSP_RD=(WAIT+1)/ipg_clk_freq, should be >= 150 ns
// [22.7] RELAX = tSP_PGM=tHP_PGM=(RELAX+1)/ipg_clk_freq, should be >= 100ns
// [7818] STROBE_PROG = tPGM = [(STROBE_PROG+1) – 2×(RELAX_PROG+1)] / ipg_clk_freq (The tPGM should be configured within the range of 9000 ns < tPGM < 11000 ns, while its recommended value is 10000 ns)
// [30.3] STROBE_READ = tRD= [(STROBE_READ+1) – 2×(RELAX_READ+1)] / ipg_clk_freq (The tRD is required to be larger than 40 ns)
//
// [30.7] TIMING2.RELAX_READ = (RELAX_READ+1) / ipg_clk_freq, should be >= 10 ns.
// [1113] TIMING2.RELAX_PROG = tSP_PG_AVDD = tHP_PG_AVDD = (RELAX_PROG+1)/ipg_clk_freq, should be >= 1000 ns.
// At default, RELAX_READ is 0x03 (3) and RELAX_PROG is 0x92 (146)
//
Using the numbers above, I get:
189 nS for the WAIT (must be >= 150 nS) so ok.
22.7 nS for the RELAX (must be >= 100 nS) so NOT ok
7818 nS for the STROBE_PROG (must be >9000 and <11000) so NOT ok
30.3 nS for STROBE_READ (must be > 40 nS) so NOT ok.
I have checked the RELAX_READ and RELAX_PROG in TIMING2 register, and they are 3 and 146.
Am I totally mis-calculating this, or is there something wrong in the original code ?
解決済! 解決策の投稿を見る。
Hi Carsten, you are absolutely right, my values of thread https://community.nxp.com/message/1097911?commentID=1097911&et=watches.email.thread#comment-1097911 are not longer correct since they have changed the value tRELAX from >16,2ns to >=100ns in reference manual. As I calculated the values, I used i.MX RT1050 Processor Reference Manual Rev 0.
The values concerning refenence manual Rev.2 (if I have calculated them correctly) should be:
//TIMING_WAIT = 150ns * 132MHz - 1 = 18,8 => 19
//RELAX = 100ns * 132MHz - 1 = 12,2 => 13
//RELAX_READ = 10ns * 132MHz -1 = 0,32 => 1
//RELAX_PROG = 1000ns * 132MHz - 1 = 131
//STROBE_PROG = 10us * 132MHz + 2 * (RELAX_PROG + 1) - 1 = 10us * 132MHz + 2 * (131 + 1) - 1 = 1583
//STROBE_READ = 40ns * 132MHz + 2 * (RELAX_READ + 1) - 1 = 40ns * 132MHz + 2 * (1 + 1) - 1 = 8,28 => 9
int timing = OCOTP_TIMING_STROBE_PROG(1583) | OCOTP_TIMING_RELAX(13) | OCOTP_TIMING_STROBE_READ(9) |OCOTP_TIMING_WAIT(19); //ipg_clk=132MHz, Calculation described at Chapter 22.4.3 (Rev.2) OTP Read/Write Timing Parameters
Please let me know if you are getting same results.
Best regards
Martin
Anyone ?
Hi Carsten, you are absolutely right, my values of thread https://community.nxp.com/message/1097911?commentID=1097911&et=watches.email.thread#comment-1097911 are not longer correct since they have changed the value tRELAX from >16,2ns to >=100ns in reference manual. As I calculated the values, I used i.MX RT1050 Processor Reference Manual Rev 0.
The values concerning refenence manual Rev.2 (if I have calculated them correctly) should be:
//TIMING_WAIT = 150ns * 132MHz - 1 = 18,8 => 19
//RELAX = 100ns * 132MHz - 1 = 12,2 => 13
//RELAX_READ = 10ns * 132MHz -1 = 0,32 => 1
//RELAX_PROG = 1000ns * 132MHz - 1 = 131
//STROBE_PROG = 10us * 132MHz + 2 * (RELAX_PROG + 1) - 1 = 10us * 132MHz + 2 * (131 + 1) - 1 = 1583
//STROBE_READ = 40ns * 132MHz + 2 * (RELAX_READ + 1) - 1 = 40ns * 132MHz + 2 * (1 + 1) - 1 = 8,28 => 9
int timing = OCOTP_TIMING_STROBE_PROG(1583) | OCOTP_TIMING_RELAX(13) | OCOTP_TIMING_STROBE_READ(9) |OCOTP_TIMING_WAIT(19); //ipg_clk=132MHz, Calculation described at Chapter 22.4.3 (Rev.2) OTP Read/Write Timing Parameters
Please let me know if you are getting same results.
Best regards
Martin
Thanks a lot Martin!
I was afraid I was seriously mistaken, happy I was not wrong
I confirm the numbers above from you, fits perfectly with mine also.
I have changed my comments to this:
// Write Fuses, burn BT_FUSE_SEL (disable BT_CFG_xx pins) and burn FORCE_INTERNAL_BOOT (so that BOOT_MODE0 and BOOT_MODE1 inputs does not matter any more)
//
// Value at the start of line is [xx] which is number of nS at 132 MHz
// Timing values at 132 MHz:
// int timing = OCOTP_TIMING_STROBE_PROG(1583) | OCOTP_TIMING_RELAX(13) | OCOTP_TIMING_STROBE_READ(9) |OCOTP_TIMING_WAIT(19); //ipg_clk=132MHz, Calculation described at Chapter 22.4.3 (Rev.2) OTP Read/Write Timing Parameters
//
//
// [151] WAIT = tSP_RD=(WAIT+1)/ipg_clk_freq, should be >= 150 ns
// [106] RELAX = tSP_PGM=tHP_PGM=(RELAX+1)/ipg_clk_freq, should be >= 100ns
// [10015] STROBE_PROG = tPGM = [(STROBE_PROG+1) – 2×(RELAX_PROG+1)] / ipg_clk_freq (The tPGM should be configured within the range of 9000 ns < tPGM < 11000 ns, while its recommended value is 10000 ns)
// [45] STROBE_READ = tRD= [(STROBE_READ+1) – 2×(RELAX_READ+1)] / ipg_clk_freq (The tRD is required to be larger than 40 ns)
//
// [15.2] TIMING2.RELAX_READ = (RELAX_READ+1) / ipg_clk_freq, should be >= 10 ns.
// [1000] TIMING2.RELAX_PROG = tSP_PG_AVDD = tHP_PG_AVDD = (RELAX_PROG+1)/ipg_clk_freq, should be >= 1000 ns.
// In TIMING2, RELAX_READ is set to 0x01 (1) and RELAX_PROG is 0x92 (131)
// (At default, RELAX_READ is 0x03 (3) and RELAX_PROG is 0x92 (146))
//
I will update the numbers for 150 MHz ipg_clk shortly and give it a try (once I get some extra boards manufactured so I don't risk messing my testboard up )
Thanks a lot!
Just to wrap this up, this is the code I currently use:
//------------------------------------------------------------------------------
// Burn BT_FUSE_SEL and FORCE_INTERNAL_BOOT fuses
//------------------------------------------------------------------------------
void setFuses(void) {
// Write Fuses, burn BT_FUSE_SEL (disable BT_CFG_xx pins) and burn FORCE_INTERNAL_BOOT (so that BOOT_MODE0 and BOOT_MODE1 inputs does not matter any more)
//
// Value at the start of line is [xx] which is number of nS at 132 MHz with the timing values below
// [151] WAIT = tSP_RD=(WAIT+1)/ipg_clk_freq, should be >= 150 ns
// [106] RELAX = tSP_PGM=tHP_PGM=(RELAX+1)/ipg_clk_freq, should be >= 100ns
// [10015] STROBE_PROG = tPGM = [(STROBE_PROG+1) – 2×(RELAX_PROG+1)] / ipg_clk_freq (The tPGM should be configured within the range of 9000 ns < tPGM < 11000 ns, while its recommended value is 10000 ns)
// [45] STROBE_READ = tRD= [(STROBE_READ+1) – 2×(RELAX_READ+1)] / ipg_clk_freq (The tRD is required to be larger than 40 ns)
//
// [15.2] TIMING2.RELAX_READ = (RELAX_READ+1) / ipg_clk_freq, should be >= 10 ns.
// [1000] TIMING2.RELAX_PROG = tSP_PG_AVDD = tHP_PG_AVDD = (RELAX_PROG+1)/ipg_clk_freq, should be >= 1000 ns.
// In TIMING2, RELAX_READ is set to 0x01 (1) and RELAX_PROG is 0x92 (131)
// (At default, RELAX_READ is 0x03 (3) and RELAX_PROG is 0x92 (146))
// For 132 MHz:
// TIMING_WAIT = 150ns * 132MHz - 1 = 18,8 => 19
// RELAX = 100ns * 132MHz - 1 = 12,2 => 13
// RELAX_READ = 10ns * 132MHz -1 = 0,32 => 1
// RELAX_PROG = 1000ns * 132MHz - 1 = 131
// STROBE_PROG = 10us * 132MHz + 2 * (RELAX_PROG + 1) - 1 = 10us * 132MHz + 2 * (131 + 1) - 1 = 1583
// STROBE_READ = 40ns * 132MHz + 2 * (RELAX_READ + 1) - 1 = 40ns * 132MHz + 2 * (1 + 1) - 1 = 8,28 => 9
//
// For 150 MHz:
// TIMING_WAIT = 150ns * 150MHz - 1 = 21,5 => 22
// RELAX = 100ns * 150MHz - 1 = 14,0 => 14
// RELAX_READ = 10ns * 150MHz - 1 = 0,5 => 1
// RELAX_PROG = 1000ns * 150MHz - 1 = 149
// STROBE_PROG = 10us * 150MHz + 2 * (RELAX_PROG + 1) - 1 = 10us * 150MHz + 2 * (131 + 1) - 1 = 1763
// STROBE_READ = 40ns * 150MHz + 2 * (RELAX_READ + 1) - 1 = 40ns * 150MHz + 2 * (1 + 1) - 1 = 11,0 => 11
//
// If BT_FUSE_SEL (bit 4) is not set already then burn it (and FORCE_INTERNAL_BOOT)
if (!(SRC->SBMR2 & SRC_SBMR2_BT_FUSE_SEL_MASK)) {
//
// Based on ipg_clk = 132 MHz => 1/f = 7.576 nS
int timing = OCOTP_TIMING_STROBE_PROG(1583) | OCOTP_TIMING_RELAX(13) | OCOTP_TIMING_STROBE_READ(9) | OCOTP_TIMING_WAIT(19); //ipg_clk=132MHz, Calculation described at Chapter 22.4.3 (Rev.2) OTP Read/Write Timing Parameters
int timing2 = OCOTP_TIMING2_RELAX_READ(1) | OCOTP_TIMING2_RELAX_PROG(131);
//
// Based on ipg_clk = 150 MHz => 1/f = 6.67 nS
// int timing = OCOTP_TIMING_STROBE_PROG(1763) | OCOTP_TIMING_RELAX(14) | OCOTP_TIMING_STROBE_READ(11) | OCOTP_TIMING_WAIT(22); // ipg_clk=150MHz, Calculation described at Chapter 22.4.3 OTP Read/Write Timing Parameters
// int timing2 = OCOTP_TIMING2_RELAX_READ(1) | OCOTP_TIMING2_RELAX_PROG(131);
//
OCOTP->TIMING = timing;
OCOTP->TIMING2 = timing2;
while ((OCOTP->CTRL & (1<<OCOTP_CTRL_BUSY_SHIFT)) || (OCOTP->CTRL & (1<<OCOTP_CTRL_ERROR_SHIFT))); // Check that HW_OCOTP_CTRL[BUSY] and HW_OCOTP_CTRL[ERROR]are clear
int ocotp_ctrl = OCOTP->CTRL;
ocotp_ctrl &= ~OCOTP_CTRL_ADDR_MASK;
ocotp_ctrl |= OCOTP_CTRL_ADDR(6); // Set address 6
ocotp_ctrl &= ~OCOTP_CTRL_WR_UNLOCK_MASK ;
ocotp_ctrl |= OCOTP_CTRL_WR_UNLOCK(0x3E77); // WR_UNLOCK sequence
OCOTP->CTRL = ocotp_ctrl; // Write ADDR and unlock
//OCOTP->DATA = (long)((1<<4)|(1<<16));// burn both BT_FUSE_SEL (1<<4) and FORCE_INTERNAL_BOOT (1<<16)
OCOTP->DATA = (long)((1<<4));// burn only BT_FUSE_SEL (1<<4)
}
}