Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

ソリューションへジャンプ
1,290件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi,

      In RT1052 RM, there is a bit to control switch from VDD_HIGH_IN to VDD_SNVS_IN, could you help to provide detailed description of the controlling circuit?

   Capture.PNG

Best Regards,

Fred Fu

0 件の賞賛
返信
1 解決策
1,280件の閲覧回数
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,287件の閲覧回数
wayne_wang
NXP Employee
NXP Employee

there is a internal diode between VDD_HIGH_IN and VDD_SNVS_IN, and this switch has function only in VDD_HIGH_IN and VDD_SNVS_IN powered, otherwise, it will always enable.

0 件の賞賛
返信
1,282件の閲覧回数
fredfu
NXP Employee
NXP Employee

Hi  Wayne,

    Thanks. Can the switch be disabled? if customer don't need the channel from VDD_HIGH_IN to VDD_SNVS_IN.

Best Regards,

Fred Fu

0 件の賞賛
返信
1,281件の閲覧回数
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

0 件の賞賛
返信