Starting co-ordinate of screen is shifting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Starting co-ordinate of screen is shifting

1,626件の閲覧回数
pavithrat
Contributor II

I am continuously reading the data and displaying it in 5 different text boxes with different colors. But the screen gets shifted from its original position after displaying it for 4-5 times. Please find attached snaps showing two different screens.

I am using i.MXRT1050 EVKB device with emwin version 5.38.


Please provide the suggestions to solve this problem.

4 返答(返信)

1,478件の閲覧回数
pavithrat
Contributor II

Gentle reminder!

1,478件の閲覧回数
b36401
NXP Employee
NXP Employee

Also it is possible that you may run into issues with weak powering your board from the USB port of the PC. Please try to use another power source.

0 件の賞賛
返信

1,478件の閲覧回数
pavithrat
Contributor II

Hello Victor,

We tried using new SDK of version 2.4.0, but the problem still exists. We are using external 5V power supply as power source instead of USB port.

Regards,

Pavithra T

0 件の賞賛
返信

1,478件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try to use latest MCUXpresso SDK you can get here:
https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-t...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信