Starting co-ordinate of screen is shifting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Starting co-ordinate of screen is shifting

1,625 Views
pavithrat
Contributor II

I am continuously reading the data and displaying it in 5 different text boxes with different colors. But the screen gets shifted from its original position after displaying it for 4-5 times. Please find attached snaps showing two different screens.

I am using i.MXRT1050 EVKB device with emwin version 5.38.


Please provide the suggestions to solve this problem.

4 Replies

1,477 Views
pavithrat
Contributor II

Gentle reminder!

1,477 Views
b36401
NXP Employee
NXP Employee

Also it is possible that you may run into issues with weak powering your board from the USB port of the PC. Please try to use another power source.

0 Kudos
Reply

1,477 Views
pavithrat
Contributor II

Hello Victor,

We tried using new SDK of version 2.4.0, but the problem still exists. We are using external 5V power supply as power source instead of USB port.

Regards,

Pavithra T

0 Kudos
Reply

1,477 Views
b36401
NXP Employee
NXP Employee

Please try to use latest MCUXpresso SDK you can get here:
https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-t...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply