Setting Timer in Low Power Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting Timer in Low Power Mode

Jump to solution
511 Views
frozen
Contributor III

I use imxrt1176, can I set timer to wake up mcu for 24 hours ?

0 Kudos
Reply
1 Solution
493 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!

View solution in original post

1 Reply
494 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!