Setting Timer in Low Power Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting Timer in Low Power Mode

ソリューションへジャンプ
533件の閲覧回数
frozen
Contributor III

I use imxrt1176, can I set timer to wake up mcu for 24 hours ?

0 件の賞賛
返信
1 解決策
515件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!

元の投稿で解決策を見る

1 返信
516件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! The first way that comes to my mind is using the GPT timer as a wakeup source, for more detail please refer to app note AN13104 Debug and Application for i:MX RT1170 Clock and Low Power Feature. If the clock and the prescaler are not slow enough, the GPT counter can be operated using an external clock (GPT_CLK) from outside the device, which in turn can be generated with another timer.

Hope it helps you.

Have a nice day!