Reallocating the flexRAM for MIMXRT1062

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reallocating the flexRAM for MIMXRT1062

822件の閲覧回数
yalin_10
Contributor II

Hi 

I am working on the MIMXRT1062. 

The SRAM_DTC is overflowed "SRAM_DTC". I tried to double the SRAM_DTC to 256KB and decrease the SRAM_OC accordingly(below). After that, the debugger stops working.

I have already tried this way - link 

1. How to reallocate FlexRAM for MIMXRT1062.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

814件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yalin_10 ,

  Which IDE and debugger you are using now?

  Which situation following you are using?

kerryzhou_0-1685002487265.png

You may select item 8, or 9.

If you use the mcuxpresso IDE and CMSIS DAP, you also need to modify the script file for the debugger with the reallocated flexRAM configuration.

 

Best Regards,

Kerry

 

0 件の賞賛
返信

793件の閲覧回数
yalin_10
Contributor II

Hi @kerryzhou 

After following the below mentioned procedure, board isn't responding, I changed those register values using NXPBootUtility

 

0 件の賞賛
返信

767件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @yalin_10 ,

  Do you mean MCUbootutility?

  As you change the fuse for the reallocation? You didn't change the register with code? Then you boot from fuse?

 

Best Regards,

Kerry

0 件の賞賛
返信