Hi
I am working on the MIMXRT1062.
The SRAM_DTC is overflowed "SRAM_DTC". I tried to double the SRAM_DTC to 256KB and decrease the SRAM_OC accordingly(below). After that, the debugger stops working.
I have already tried this way - link
1. How to reallocate FlexRAM for MIMXRT1062.
Hi @yalin_10 ,
Which IDE and debugger you are using now?
Which situation following you are using?
You may select item 8, or 9.
If you use the mcuxpresso IDE and CMSIS DAP, you also need to modify the script file for the debugger with the reallocated flexRAM configuration.
Best Regards,
Kerry
Hi @kerryzhou
After following the below mentioned procedure, board isn't responding, I changed those register values using NXPBootUtility
Hi @yalin_10 ,
Do you mean MCUbootutility?
As you change the fuse for the reallocation? You didn't change the register with code? Then you boot from fuse?
Best Regards,
Kerry