RT1176 Inductor for the internal DC-DC Converter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1176 Inductor for the internal DC-DC Converter

463 次查看
Wobaffet
Senior Contributor I

Hello, 

For our project, we'll be using RT1176 MCU, on the design for the evk there is a 4.7uH inductor which is this: 74404041047 from würth. Instead of this can we use one of the alternatives below?

SRP0420-4R7K from Bourns Inc.

DFE322520FD-4R7M=P2 from Murata

Thank you in advance!

Best Regards.

0 项奖励
回复
1 回复

439 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

NXP does not recommend any component that is not an NXP product. The recommended value for the external inductor is about 4.7 μH with the saturation current > 1.5 A and ESR < 0.1 Ω.

Hope it helps you.

Have a nice day!

0 项奖励
回复