RT1170 SEMC CE# timing of SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 SEMC CE# timing of SRAM

Jump to solution
753 Views
Eugene3
Contributor II

Hi

Is it possible to output ADDRESS before CE# assert?

As far as I confirmed, CE# assertion is min 1 clock earlier than ADDRESS assertion on SRAMCRx register.

 

0 Kudos
Reply
1 Solution
709 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 

No, it is not possible, at minimal , the CE# setup time is 1 clock and the address line setup is 1 clock as well.

Kan_Li_0-1695025980953.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
710 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

 

No, it is not possible, at minimal , the CE# setup time is 1 clock and the address line setup is 1 clock as well.

Kan_Li_0-1695025980953.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
690 Views
Eugene3
Contributor II

Thank you, I understand.

0 Kudos
Reply