RT1170 GPIO Operating Range setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1170 GPIO Operating Range setting

跳至解决方案
1,010 次查看
Eugene3
Contributor II

How can I set 3.3V mode or 1.8V mode for GPIO_SD?

GPIO_LPSR, AD and DISP have register for supply voltage range selection. But I couldn't find similar register for GPIO_SD and EMC.

Is the mode simply selected by the NVCC_XX power rail voltage without register setting?

0 项奖励
回复
1 解答
956 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

The pad work in 3.3v mode or 1.8v mode is designed by hardware. NVCC_SD is the power source of SD pin group. You can refer to RT1170 EVK schematic for how to switch.

jingpan_0-1694670727224.png

 

Regards,

Jing

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
957 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

The pad work in 3.3v mode or 1.8v mode is designed by hardware. NVCC_SD is the power source of SD pin group. You can refer to RT1170 EVK schematic for how to switch.

jingpan_0-1694670727224.png

 

Regards,

Jing

 

0 项奖励
回复
950 次查看
Eugene3
Contributor II

Hi @jingpan 

Can I also apply same way to other power rails to set 1.8V/3.3V mode?

ex. If I use 1.8V power to NVCC_EMC1, will GPIO_EMC_B1_XX work in 1.8V range?

0 项奖励
回复
899 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

Yes, it can.

 

Regards,

Jing

0 项奖励
回复
858 次查看
Eugene3
Contributor II

Thank you.

I understand.

0 项奖励
回复