RT1064 RT1050 ADC VDDA_ADC_3P3 Supply Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1064 RT1050 ADC VDDA_ADC_3P3 Supply Current

539件の閲覧回数
andyhewitson
Contributor I

Hi,

Working on a new RT1064 design.  Since Vrefh is bonded to VDDA_ADC_3P3, I'd like to drive VDDA_ADC_3P3 with a reference, instead of using the [relatively] noisy 3.3V supply.

I'm struggling to find a supply requirement for VDDA_ADC_3P3.  Page 23 of IMXRT1064CEC says that max is 40mA.  If I'm reading it correctly, 33mA of that is for the resistive touch screen (worst case).  I'm not using the Touch Screen Controller.  Does that mean that without the TSC, VDDA_ADC_3P3 max is 7mA for both converters running at 1MS/s?  Seems a bit light.

TIA, Andy.

ラベル(2)
0 件の賞賛
返信
1 返信

494件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Running at running at 1MS/s is not specified. However, you can find more details of typical values and conditions in Table 55. 12-bit ADC characteristics (VREFH = VDDA, VREFL = VSSAD) of the datasheet.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信