RT1021 BEE encryption problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1021 BEE encryption problem

2,392 Views
claire_chen
Contributor I

Hello,

RT1021 BEE encryption problem
The demo uses the RT1021-EVK, SDK code: hello world to perform XIP encrypted (BEE user keys) authenticated encryption using MCUXpresso Secure Provisioning Tool, but the board does not run, the attachment is the operation The attached is the procedure. Please help to see what causes the problem, thanks!

claire

0 Kudos
Reply
7 Replies

2,390 Views
claire_chen
Contributor I

Adding the attachment.

0 Kudos
Reply

2,313 Views
kerryzhou
NXP TechSupport
NXP TechSupport

楼主你好!

我发现你SW8配置不对,您试试这个:

通过查看所有烧录后的image,复位设备,改变板子启动模式为boot from internal模式,BT_CFG[0]=1,即(SW8 1-ON, 2-OFF, 3-ON, 4-OFF) 然后断电,重新上电。发现LED闪烁,所以可以说明BEE加密已经工作。

看看是否能启动?

如果不行,你就用我case里面的软件。

Best Regards,

Kerry

0 Kudos
Reply

2,369 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @claire_chen ,

   In the previous time, I do the RT1020 BEE on my side.

   You can refer to my post:

https://www.nxpic.org.cn/module/forum/thread-619420-1-1.html

   As you are from China, you also can read the Chinese doc.

 

After you read it, if you still have issues, just kindly let me know.

Best Regards,

Kerry

0 Kudos
Reply

2,335 Views
claire_chen
Contributor I

Hi kerry,

    Thank you for your reply. We have already referred to this post before, but it still has the same phenomenon. The writing was successful, but the encryption was not successful, and the code cannot run.

claire chen

0 Kudos
Reply

2,332 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @claire_chen ,

    If that method also can't works, Your chip may mistakely operated.

   Do you have any new chip to test it on your side or not?

   You can create an private case, then I can share my testing file to you, as it can't put in the public side.

 

Best Regards,

Kerry

0 Kudos
Reply

2,321 Views
claire_chen
Contributor I

Hi Kerry,

     The case number is 00537721

     Please help provide the test file.Thanks!

Claire 

 

0 Kudos
Reply

2,315 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @claire_chen ,

   Thanks for your cooperation, I already take your case, will reply you in the case.

 

Best Regards,

Kerry

0 Kudos
Reply