RT1011 on the configuration of ONOFF pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1011 on the configuration of ONOFF pins

929件の閲覧回数
tim-wei
Contributor I

I use RT1011 to achieve the function of low power consumption, but there is no wakeup pin to wakeup. Now I want to use ONOFF.
1. Use software control to shut down or sleep the MCU.
2. Make the ONOFF pin receive external signals, and turn on or wake up the MCU in the previous step.
It is not known how these functions are implemented and there is no relevant reference code.
After looking at the SVNC code, ONOFF and low power seems to be different.

谢谢

0 件の賞賛
返信
1 返信

917件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you to refer to the application note: https://www.nxp.com/docs/en/application-note/AN12085.pdf

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信