Put a API run in SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Put a API run in SRAM

1,132 Views
kensu
Contributor V

Hi, I am using 1015RT, my boot image is serial nor flash,

To improve the performance, I want to put a API running in SRAM from flash,

How to do it?

Is a simple way to make it?

Thanks

Ken

Labels (2)
0 Kudos
Reply
4 Replies

1,035 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer below document about how to relocate code with MCUXpresso IDE:

https://community.nxp.com/docs/DOC-335283 

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,035 Views
kensu
Contributor V

Hi Mike

Thanks for your reply,

I know these setting can work for LPC series MCU.

I want to double confirm can it also use on i.MX RT series MCU?

Regards

Ken

0 Kudos
Reply

1,035 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Ken,

Yes, it is same to relocate a API in RAM for RT & LPC product with MCUXpresso IDE.

Thanks.

best regards,

Mike

0 Kudos
Reply

1,035 Views
kensu
Contributor V

Hi Hui_Ma

Thanks a lot for your reply.

Best Regards

Ken

0 Kudos
Reply