Probe to target MIMXRT1010 not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Probe to target MIMXRT1010 not available

6,692 Views
udayatejwani
Contributor I

Hi,

The probe is not available.  I have attached a picture.

nxpprobe.png

Also, the target being displayed is MIMXRT1011xxxx instead of MIMXRT1010.  Please help.

Thanks,

Udaya

Labels (1)
0 Kudos
Reply
3 Replies

1,179 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi udaya:

 

I would suggest you delete the existing launch configuration , then a debug probe discovery operation will be automatically performed to display the available debug connections.

 

Please refer to below link for more details.

MCUXpresso IDE: Debug Probe Selection Dialog (Probe Discovery) 

 

 

Regards

Daniel

1,179 Views
udayatejwani
Contributor I

The above suggestion did not work.  When I invoke MCUExpresso, I get a message that crt_directory2.xme is not found at the usual places.  Could that be the cause?  How can I fix it?

Regards,

Udaya

0 Kudos
Reply

1,179 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Udaya:

Please refer to this file as attached, it is from my installation folder.

Location is :

MCUXpressoIDE_11.1.0_3209\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.1.0.201912041804\binaries

MCUXpresso IDE 11.1.0 is the latest version, it can be downloaded from

MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP 

Regards

Daniel

0 Kudos
Reply