使用OpenOCD调试RT1052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

使用OpenOCD调试RT1052

1,259 Views
1318614689
Contributor II

我使用VisualGDB为RT1052编写程序并下载调试,但是VisualGDB使用OpenOCD调用CMSIS DAP下载器,它需要一个cfg脚本文件,请问NXP公司有对此的支持吗

Labels (2)
0 Kudos
Reply
1 Reply

1,170 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

非常感谢使用NXP产品,很高兴为你提供技术支持!
抱歉,NXP公司无这方面的支持。

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply