I'm running into a few problems getting started with my MIMXRT1020EVK, so I decided to just follow the steps in the "Flashloader Use Case" document that comes with the flashloader package for the MIMXRT1020EVK (Flashloader_RT1020_1.0_GA)...
Referring to that document and the directory that comes with the package, I ran the following commands:
Each of these commands worked, but the sanity test (as per the document) failed...
The USB port is apparently supposed to re-enumerate to a different VID/PID, but it doesn't.
Any ideas?
Solved! Go to Solution.
Turns out that the addresses passed to sdphost are different. For details on that refer to this post.
In the nutshell...
work much better. Thanks to the originator of that post.
Turns out that the addresses passed to sdphost are different. For details on that refer to this post.
In the nutshell...
work much better. Thanks to the originator of that post.