Hi
We are planning on re-engineering project which requires migration from K70 MCU to IMX6 RT processor
The existing K70 MCU has MXQ RTOS
Can you please let me know if MXQ RTOS is supported by IMX6 RT and could be easily migrated from K70 to IMX6 RT
Hello danielchen,
As you mention "MQX v5 supported devices are I.MX 6SX and I.MX6ULL".
Is it also supported I.MX6UL?
Hi @shrinivasnh :
Just as Jay mentioned. MQX 4.x not support I.MX RT.
There is a MQX v5 version, it is a continuation of the MQX Classic product available under low-cost commercial license terms. Supported devices includes RT 1170/1064/1050/1060/1020/1024/....
I.MX 6SX and I.MX6ULL also supported
Please refer to below link for more details.
Regards
Daniel
MQX RTOS is not supported in i.MX6 RT SDK, Azure-RTOS and FreeRTOS are supported.
You need to port MQX to i.MX6 RT by yourself, although K70 is totally different from i.MX6 RT, but RTOS is not strictly related to MCU device