【MIXMRT1061DVL6B】AVB Daisy chain connection of MIXMRT1061DVL6B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

【MIXMRT1061DVL6B】AVB Daisy chain connection of MIXMRT1061DVL6B

跳至解决方案
1,527 次查看
bobhi009
Contributor I

Hello;

    Does the two Ethernet controller of MIXMRT1061DVL6B with support for IEEE1588 support daisy chain connection , to transmit audio data and control data。

标签 (1)
0 项奖励
回复
1 解答
1,509 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 

 All the audio code, you can find it in the SDK  USB area, or the sai driver project. we didn't provide 3rd part lib.

  Yes, no directly DMIC, RT600/500 contains it. Normally, to record the audio, we use the I2S in the SAI module.

Wish it helps you!

Best Regards,

Kerry

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,521 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 

    RT1061 contains 2 ethernet, normally, one ethernet connect to one PHY, then connected externally to the ethernet interface.

    I am not sure which detail daisy chain connection you mentioned, do you want to connect two ethernet pin together without the PHY? Then do the 2 ENET communication in one R1061 chip? Can you draw one simple picture about your desired connection? Thanks.

best Regards,

Kerry

0 项奖励
回复
1,516 次查看
bobhi009
Contributor I

kerry:

     thanks for your replay. I want to make a device like the picture show, the pc can play a sound with the usb , And all device can play it to speaker,  and all device pdm mic can be captured by PC with USB.  

 

bobhi009_0-1628663856047.png

 

0 项奖励
回复
1,514 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 ,

    I think you still need to connect the PHY,  Dev1_ENET1->PHY->PHY->Dev2_ENET2, I think this method should be OK, as it is mainly using the enet to do communication between the different RT chip, if just pin to pin connection between the different RT chip, I think that is not supported.

   To the USB, it's OK to use it.

 

Best Regards,

kerry

0 项奖励
回复
1,511 次查看
bobhi009
Contributor I

kerryzhou:

      Yes ,need to connect the PHY. the other question is do we need additional third-party libraries to achieve audio synchronization between different devices? Is there any reference material?And I noticed that this chip does not have a DMIC interface, Do you need to use SPI to simulate receiving PDM data, and then do the PDM to PCM conversion on the software?Any suggestions in this ?

     

 

0 项奖励
回复
1,510 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @bobhi009 

 All the audio code, you can find it in the SDK  USB area, or the sai driver project. we didn't provide 3rd part lib.

  Yes, no directly DMIC, RT600/500 contains it. Normally, to record the audio, we use the I2S in the SAI module.

Wish it helps you!

Best Regards,

Kerry

0 项奖励
回复