MIMXRT1170-EVKB and 1XK M.2 Module...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1170-EVKB and 1XK M.2 Module...

ソリューションへジャンプ
1,588件の閲覧回数
application_ninja
Contributor III

What is required, and where is the documentation, on how to get the 1XK M.2 module to work with the MIMXRT1170-EVKB kit?

0 件の賞賛
返信
1 解決策
1,551件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

The guide is available in previous SDK releases but for some reason not in SDK 2.14.0. I am already taking action to notify this to the corresponding team.

 

Regards,

Daniel.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,579件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I would recommend you to download the whole RT1170 EVK SDK. You can find all the documentation related to Wi-Fi and Bluetooth in the following path <SDK_PATH> \docs\wireless\.

 

I really hope this helps.

Regards,

Daniel.

0 件の賞賛
返信
1,575件の閲覧回数
application_ninja
Contributor III

But the kits are different, and I believe you have to remove resistors / add resistors, etc... not sure exactly what is required for the newer EVKB board, thus my question...

0 件の賞賛
返信
1,567件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

According to the documentation form the SDK, there is no HW rework needed in order to use Wi-Fi in the RT1170-EVKB and 1XK.

If you are planning to use Bluetooth, a HW rework is needed to enable the HCI UART and PCM interface. You can find this rework explained in the Hardware Rework Guide for EdgeFast BT PAL. You can find it in your SDK bundle.

Regards,

Daniel.

0 件の賞賛
返信
1,560件の閲覧回数
application_ninja
Contributor III

That document is not within the RT1170-EVKB NXP SDK. I do however have the Embedded Artists SDK installed, and it is available there. But it should be included in the NXP SDK, I would think?

0 件の賞賛
返信
1,552件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

The guide is available in previous SDK releases but for some reason not in SDK 2.14.0. I am already taking action to notify this to the corresponding team.

 

Regards,

Daniel.

0 件の賞賛
返信
1,058件の閲覧回数
MNNgyn
Contributor II

Hey Daniel,

I am having trouble finding the SDK examples for Edgefast Bluetooth on MIMXRT1170-EVK. I saw it was present in version 2.13 but not in 2.15. I was wondering if you have any ideas why there are no EdgeFast Bluetooth examples on MIMXRT1170-EVK?

988件の閲覧回数
Kbrannan
Contributor II

I also was wondering why the newer release didn't have Edgefast examples. EVKB 2.15.00 has it included, but not the regular EVK.

 

0 件の賞賛
返信