MIMXRT1062xxx5A Startup Current Consumption

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1062xxx5A Startup Current Consumption

584件の閲覧回数
Rudy25
Contributor I

Hi all,

One of our project is using the NXP MIMXRT1062xxx5A. We have noticed that the current consumption at 3.3V is different when powering up the board the first time and when firmware upgrade is done via the flashloader and the board boot-up again after firmware upgrade is done.

When I say, 3.3V it means the voltage rail to power the DCDC_IN, VDD_HIGH_IN, VDDA_ADC_3P3, VDD_SNVS_IN, NVCC_SD1, NVCC_SD0,, NVCC_GPIO, NVCC_EMC of the microcontroller.

We put a DMM in series across 3.3V to measure the current and we are getting different results as follows.

A. The board is OFF then we supply power to the board. The board will boot-up and we are reading around 35mA.

B. The board is ON and running. We trigger a firmware upgrade request and then it jumps from Application to Bootloader. The flashloader will run then to perform the firmware upgrade. Once firmware upgrade is done, the board will boot-up and during this time we are reading around 45mA.

Where is this 10mA difference coming from? Any help or idea is greatly appreciated.

 

Thank you.

Regards,

Rudy

 

 

0 件の賞賛
返信
2 返答(返信)

525件の閲覧回数
Rudy25
Contributor I

Hello @EdwinHz,

Thanks for your response.

Yes, the current consumption remains at 45mA after firmware upgrade where MCU did reset.

But it is different if I manually reset the power supply. The current consumption is only 35mA.

 

 

0 件の賞賛
返信

539件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Rudy25,

This extra consumption is natural during firmware upgrade due to the natural processing power and peripheral activation.

However, did I understand that current consumption remains at 45mA after MCU reset as well?

0 件の賞賛
返信