MIMXRT1020-EVK rev A3 Schematics

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIMXRT1020-EVK rev A3 Schematics

跳至解决方案
3,975 次查看
amczarny
Contributor I

Hi, I have a dev board MIMXRT 1020-EVK rev A3 but I can not find a schematics for that revision. The https://www.nxp.com/webapp/Download?colCode=MIMXRT1020-EVK-Design-Files has rev B1 which has different jumpers setup (j25, j26 etc) and debugger chip. Can you please provide me with schematics for rev A3

标记 (2)
0 项奖励
回复
1 解答
3,949 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

在原帖中查看解决方案

8 回复数
3,007 次查看
mcampani72
Contributor I

Here are the schematics.

Regards

 

0 项奖励
回复
3,482 次查看
bretts
Contributor I

I have a Rev A3 board that I also need the schematics for, could you please provide them?

 

Thanks,

 

Brett Swimley

0 项奖励
回复
3,946 次查看
amczarny
Contributor I

Thanks, highly appriciated

0 项奖励
回复
3,950 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

3,026 次查看
EB_A
Contributor I

I've the same issue I'm not able to find correct information on schematics and jumper present in the rev 3 board..

May you provide schematics ?

Emilio

0 项奖励
回复
3,314 次查看
bikenomad
Contributor IV

I need this schematic too.

0 项奖励
回复
3,549 次查看
andong
Contributor I

I have RevA3 board too, i need the schematics of the same , Can i please get it?

0 项奖励
回复
3,600 次查看
vrajesh
Contributor I

I have RevA3 board, i need the schematics of the same , Can i please get it.

0 项奖励
回复