Dear support,
I am learning i.MXRT MCUs with RT1170-EVK boards, I am using MCUXpresso SDK 2.11 on Ubuntu with ARMGCC 10.2. and CMake tools. My board has been set to boot from octal flash.
I have a very simple RTT demo program and I can build programs with different build types successfully.
However, the program from "flexspi_nor_sdram_debug" build couldn't reach my "main()" function even inside a gdb session. I've attached the .elf program and my build and gdb session logs in "octal_sdram_err.bz2" for your review.
Regards,
yf2
解決済! 解決策の投稿を見る。
Okay, I have created new ticket for SDKv2.12 and will close this ticket soon, please help to check that ticket.
Regards,
yf2
Hi @yf2 ,
Thanks for your new question post.
To be honesty, I don't have the Ubuntu test platform.
But I am familiar with the windows+RT1170+octal flash.
About your RTT demo, do you use the SDRAM or not? If not, you don't need to add DCD area, if yes, you still need to add the DCD configuration, which is the SEMC configuration for the SDRAM.
About your RTT demo, when need to download to the octal flash, you still need to modify the FCB to the octal flash, about the FCB related file, I already share with you in another post previously.
So, now, I think, maybe you can generate the RTT demo .bin or srec file, and test it on the windows system, make sure that image is working with the octal flash, then you can switch to your Ubuntu system, as you are more familiar with Ubuntu system.
Best Regards,
Kerry
My hello_rtt program is based on hello_world demo, the main difference is that hello_rtt doesn't use debug console but uses RTT console for logging.
During my learning process, I noticed that there are different linker descriptor files in armgcc/ folder:
$ ls *.ld
MIMXRT1176xxxxx_cm7_flexspi_nor.ld
MIMXRT1176xxxxx_cm7_flexspi_nor_sdram.ld
MIMXRT1176xxxxx_cm7_sdram.ld
MIMXRT1176xxxxx_cm7_sdram_txt.ld
MIMXRT1176xxxxx_cm7_ram.ld
From the CMake scripts file, I learnt that I have tried the first and last linker descriptors already with "debug" and "flexspi_nor_debug" built types. Then I wanted to try more build types.
From the rest linker descriptor file names, I can see "sdram" is contained by all the rest three other linker files.
So even though my program doesn't explicitly require SDRAM, these linkers may require to use SDRAM. For example, maybe they want to map functions or global data of my program to SDRAM address space.
By default, my hello_rtt program doesn't require to use "dcd.c" but without it the linker complained that "dcd_data" is undefined reference. So I tried two ways to resolve it:
So if you know any links or guides about how to build and run programs in SDRAM, please teach and I can see what to do from there.
Regards,
yf2
Hi @yf2 ,
Please tell me, the SDK original hello_world demo work Ok or not on your side with DCD?
If your hello_rtt don't use the SDRAM, you can set the define:
XIP_BOOT_HEADER_DCD_ENABLE =0, then build the project again, it will without the DCD area for the SDRAM.
You can check your code setting, whether this method works OK on your side or not.
Best Regards,
KERRY
>>> Please tell me, the SDK original hello_world demo work Ok or not on your side with DCD?
My answer is no. You can confirm it with hello_world/cm77/armgcc/build_sdram_debug.bat script and see if the program can run with JLink.
Here it can't enter the main() function with JLinkGDBServerCL v7.66a.
Regards,
yf2
Hi @yf2 ,
Thanks for your information.
Ok, I get it, when I have time, I will establish the ARMGCC platform to test it. Recently, really a lot of cases in the queue to test.
Now, could you please help to test this code:
\SDK_2_11_1_MIMXRT1170-EVK\boards\evkmimxrt1170\demo_apps\led_blinky
Still the same, change FCB to octal flash which I told you, this project didn't add the SDRAM, whether it works on your side with JLINK or not?
Just to confirm it.
Best Regards,
Kerry
Kerry
Yes,. the led_blinky demo app can be programed to cctal flash by JLink using your RT-URL-Kerry device driver and it can run well.
Regards,
yf2
Hi @yf2 ,
Thanks good! So, it makes things a little easy now.
To the helloworld, you can check the define, set this one in the complie define:
XIP_BOOT_HEADER_DCD_ENABLE =0,
Then, it will help you commend the SDRAM related code, then it should also works like the led_blinky.
If you don't need the SDRAM, just check it. For the build type, also use the same as the led_blinky instead of the sdram_debug.
If you need the SDRAM, please also let me know.
Best Regards,
Kerry
Actually I need all ARMGCC build types of hello_world app can work. There are five build types as I listed above, two build types (debug and flexspi_nor_debug) already work. The other three types (sdram, sdram_txt and nor_sdram) doesn't work now.
Since hello world is a part of the SDK release, it is better to work in all types so that we can learn more from it. The iled_blinky has less build types and its "sdram" build type doesn't work either.
So the problem seems to be like:
- "sdram" related ARMGCC build types can't build workable SDK sample apps.
I do need to explore the SDRAM usage so that to better understand the RT117x device. So please help when you are free later.
Regards,
yf
Hi @yf2 ,
Thanks for your information!
Ok, clear, I will find time to establish the platform and test it.
Best Regards,
Kerry
Hi @yf2 ,
I am so sorry for the later reply! It's my mistake to miss the testing, as recently, too many cases were in the testing queue.
I will use the newest SDK 2.12.0 to test it these days.
If you have time, please also try the newest SDK2.12.0, thanks.
If it's OK could you please create a new question post about this post to continue it, and let me know, as we can't open one post so a long time.
Thanks a lot for your understanding.
Best Regards,
Kerry
Okay, I have created new ticket for SDKv2.12 and will close this ticket soon, please help to check that ticket.
Regards,
yf2