Good day,
We are developing a product that uses the MIMXRT1062DVL6B together with IS25WX256-JHLE flash. It is a custom board, but we have verified that booting from flash is working with a basic LED blinking firmware, flashed via USB with NXP MCU BootUtility v6.2.0.
We set the Device Model to "ISSI_OctalSPI_IS25LXxxx_IS25WXxxx", and only change the frequency 30 MHz.
Now that we continued development we encountered two separate problems:
1: The ROM bootloader refuses to boot an image larger than 128KiB
Firmware smaller than 128K boots without a problem, but anything larger and the firmware does not boot (attaching debugger shows only code from ROM area is running).
We rule out other issues by making a simple change:
We patch the "length" field in boot_data to a number below 128K:
boot_data at 0x60001020
uint32_t start
uint32_t length <-- Only patched this from 200K to 30K!
uint32_t plugin
Then, the firmware boots up without issue, even though it actually is larger! Areas above 128K in the flash are accessible by the firmware without a problem.
So now we can boot larger images, but it feels like a bad hack. What's the problem?
2: Flashing via J-Link does not work
Being able to use J-Link and Ozone debugger for flashing would greatly help with development.
How do we get this working smoothly?
We have tried the builtin-in flashloader from SEGGER as well as RT-UFL.
I have described the issue here in more detail: https://github.com/JayHeng/RT-UFL/issues/16
已解决! 转到解答。
Alright, I have written a minimal flashloader from scratch which seems to be working.
Important points for other people finding this thread:
Basic code to get started on the flashloader:
serial_nor_config_option_t option;
option.option0.U = 0xC0603001;
option.option1.U = 0;
// NOTE(robin): Reset the flash chip as it may be in an invalid state.
BOARD_INITPINS_FLASH_RST_GPIO->DR_CLEAR = BOARD_INITPINS_FLASH_RST_PIN_MASK;
for(volatile int i = 0; i < 1000; ++i) {}
BOARD_INITPINS_FLASH_RST_GPIO->DR_SET = BOARD_INITPINS_FLASH_RST_PIN_MASK;
for(volatile int i = 0; i < 1000; ++i) {}
status_t volatile status = ROM_FLEXSPI_NorFlash_GetConfig(0, &flashConfig, &option);
if(status == kStatus_Success)
{
status = ROM_FLEXSPI_NorFlash_Init(0, &flashConfig);
if(status == kStatus_Success)
{
// Go nuts
}
}
Alright, I have written a minimal flashloader from scratch which seems to be working.
Important points for other people finding this thread:
Basic code to get started on the flashloader:
serial_nor_config_option_t option;
option.option0.U = 0xC0603001;
option.option1.U = 0;
// NOTE(robin): Reset the flash chip as it may be in an invalid state.
BOARD_INITPINS_FLASH_RST_GPIO->DR_CLEAR = BOARD_INITPINS_FLASH_RST_PIN_MASK;
for(volatile int i = 0; i < 1000; ++i) {}
BOARD_INITPINS_FLASH_RST_GPIO->DR_SET = BOARD_INITPINS_FLASH_RST_PIN_MASK;
for(volatile int i = 0; i < 1000; ++i) {}
status_t volatile status = ROM_FLEXSPI_NorFlash_GetConfig(0, &flashConfig, &option);
if(status == kStatus_Success)
{
status = ROM_FLEXSPI_NorFlash_Init(0, &flashConfig);
if(status == kStatus_Success)
{
// Go nuts
}
}
Hi @robvos
Q1. It's strange for this case, it should be workable based on the hardware. Would you please try use MCUXpresso to double check if it is work?
BTW, "We set the Device Model to "ISSI_OctalSPI_IS25LXxxx_IS25WXxxx", and only change the frequency 30 MHz." How to change and what's the meaning?
B.R
Sam
BTW, "We set the Device Model to "ISSI_OctalSPI_IS25LXxxx_IS25WXxxx", and only change the frequency 30 MHz." How to change and what's the meaning?
This is what I configure in the NXP MCU Boot Utility.
Would you please try use MCUXpresso to double check if it is work?
Flashing via MCUXpresso does not work. Using the "GUI Flash Tool" button results in an error:
Hi @robvos
I double checked with NXP MCUXpresso (default is CMSIS-DAP), it doesn't directly support Octal flashloader (MCUXpressoIDE_11.9.1_2170\ide\LinkServer\Examples\Flashdrivers\NXP\iMXRT).
Plz try with the attchement (for RT1170) from link https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT1170-Octal-flash-enablement/ta-p/1498369 and https://github.com/JayHeng/RT-UFL/blob/master/README-en.md for reference.
I checked with the author of MCUBootUtility and RT-UFL about the two questions, it should work well without any 128KB limitation.
B.R
Sam
Thank you for the link.
So to be clear, this is what I should have?
<Device>
<ChipInfo Vendor="NXP"
Name="MIMXRT1062_UFL_octalFlash"
WorkRAMAddr="0x20200000"
WorkRAMSize="0x00040000"
Core="JLINK_CORE_CORTEX_M7"
Aliases="MIMXRT1062_Octal" />
<FlashBankInfo Name="Octal Flash"
BaseAddr="0x60000000"
MaxSize="0x02000000"
Loader="Devices/NXP/iMXRT_UFL/MIMXRT_FLEXSPI_UV5_UFL.FLM"
LoaderType="FLASH_ALGO_TYPE_OPEN" />
</Device>
In the J-Link pop-up, the Compare fills to 100% but then fails to erase:
Device "MIMXRT1062_OCTAL" selected.
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Cache: L1 I/D-cache present
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
[0][0]: E00FE000 CID B105100D PID 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
[1][0]: E00FF000 CID B105100D PID 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
[2][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[2][1]: E0001000 CID B105E00D PID 000BB002 DWT
[2][2]: E0002000 CID B105E00D PID 000BB00E FPB-M7
[2][3]: E0000000 CID B105E00D PID 000BB001 ITM
[1][1]: E0041000 CID B105900D PID 001BB975 ETM-M7
[1][2]: E0042000 CID B105900D PID 004BB906 CTI
[0][1]: E0040000 CID B105900D PID 000BB9A9 TPIU-M7
[0][2]: E0043000 CID B105F00D PID 001BB101 TSG
I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Connected to target device.
J-Link/J-Trace serial number: 601014830
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Failed to erase sectors.
I also tried with MIMXRT1060_UFL_L0, which gave the same result.
I get the feeling I will need to build RT-UFL myself to debug this properly. Sadly, its build system seems to depend on either Keil MDK or IAR, which are paid solutions we do not use. So I will need to convert it first..
Hallo @robvos
We have a design with IS25WX064 which is working okay.
Regarding 2):
The Segger Flash loader does not support Octa-SPI Flash-Memory. Some IDEs use own flash-loaders which may support octa-spi (also via Segger J-Link). We also used an adapted flash-loader.
Regards