Hi All,
I tried to flash application binary on SLN-LOCAL2-IOT using MSD method. Initially the application was running in the Bank A .So I linked new image to Bank B before building the local_demo and flashed using MSD method.The changes in the application got updated in the EVK. Again I needed to change the application and hence repeated the same procedure and flashed.But changes are not getting updated on the EVK. Anything needs to be done in order to update the new image on the EVK?
Kindly help me in resolving this issue.
Thanks in advance.
Hi @jnj ,
When you run the bank A and bank B, do you use the console to check the on going app version? Whether that it is correct, if running bank A, you need to download bankB in MSD.
Now, if you can't run the app, can you enter the MSD or not?
If no, I highly suggest find an JLINK, then use the JLINK download the code directly. download both A and B app. As I always use the debugger to download the code directly.
If you still have issues, just kindly let me know.
Best Regards,
Kerry
Hi @kerryzhou ,
Thanks for the response.I could flash the EVK with application binary via debugger(SEGGER JLink).But now I am facing another issue after flashing application bin with changes.I am not even able to access the USB console and application seems to be bot running in the evk. Could you please help on this?
Thanks in advance.
Hi @jnj ,
Please also use your debugger download these two project again:
SDK_2_8_0_SLN-LOCAL2-IOT\boards\sln_local2_iot\sln_boot_apps
Then try it, whether your USB can be connected or not?
Just update all the related firmware.
Any updated information, just kindly let me know.
Best Regards,
Kerry
Hi @kerryzhou ,
I tried flashing bootloader and bootstrap multiple times.But there is no any progress?Any memory mapping needs to be done ?
Hi @jnj ,
Please check your hardware, as you know, it is using two boards insert together, whether your two boards connection is not good?
You can divide the two boards, and insert them together again.
As you know, the USB is in another board which is not the MCU board, as all your app, boot project has be programed, if the USB still not work, and you even can't find the UART, seems your board connection is not good, what about the boot mode, do you use internal boot mode, or the serial download mode?
J27 should be connected to 1.
You also can take a photo about your board, and give me the photo.
Please give me your power on photo, I need to check which led is on.
Best Regards,
Kerry
Hi @kerryzhou ,
Kindly see the attachment.
J27 is connected to 1 only. I think hardware connections are good.
Hi @jnj
Thanks for your updated information.
Your led is correct.
When you power on, the app is not run, and no voice out, right?
What about the device management, can you find the UART com port like me or not?
In your bootstrap and bootloader project, turn off the image verification.
Then use the Debugger download the code again.
to the local_demo, please download it to two different address:
Application Bank A 0x6030_0000
and Application Bank B 0x60D0_0000
In fact, I also meet one times like you, use the MSD download to the wrong area, then I also use the JLINK debugger download the following
Then the board is back to normal. When you enter the MSD, you need to power off the USB, then press the SW2 and hold it, then plug the USB.
Please give me more details about your question:USB is not getting detected in Windows PC.
Can't enter the MSD mode? Or even the UART COM also didn't work?
Best Regards,
Kerry
Hi @kerryzhou ,
I am not able to set board in MSD mode by pressing and holding SW2 and also not able to access the console(USB-CDC-ACM).
Hi @jnj
OK, now, do you remember the detail steps to damage your board? whether the related app.bin still exist?
If yes, give me the detail steps, I will follow you and test it, whether my board also the same as you or not.
provide your test image, give me details issue reproduce steps, as I have two SLN-LOCAL2-IOT, so I can help you to test it, if I also meet issues, then I can do more checking on my own side.
best Regards,
kerry
Hi @kerryzhou ,
I wanted to get the application logs.So I put a configPRINTF() in the main() function in main.c of sln_local2_iot_local_demo.Compiled the code and I have done the debug.Got Assertion failed . So I flashed both bootloader and bootstrap images using SEGGER.After that ,only flashing is working.Application seems to be not running in the evk(voice is not coming and led blinking is also not happening).Then I checked the boostrap memory map.It was on 0x6000_0000.So I changed to 0x6000_2000(mentioned in the SLN-LOCAL2-IOT-DG.pdf) and Flashed the same.But still problem exists.
Hi @jnj ,
No, boostrap memory you don't need to move to 0x6000_2000, as this project contains the FCB+IVT from 0x60000000. xip folder:hyperflash_config and image_vector_table.
Do you test my last suggestion, turn off the image verification?
Refer to chapter 5.3 Turning off image verification in the SLN-LOCAL2-IOT-DG.pdf
Please try it at first.
BTW, please also enter serial download mode, then use the MCUbootUtility tool:
https://github.com/JayHeng/NXP-MCUBootUtility/archive/refs/tags/v3.3.1.zip
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility
Your board, power off, J27 connect to 0, then power on the USB, open the MCUbootUtiliy:
Can you find the USB VID and PID?
If yes, Connect to ROM button, then use my attached .bin file, burn it to 0x60000000, length is 0x1dc0000. This .bin file is readout from my board.
The burn time is long, just wait it patiently, you can see the log window, wait it finished.
step 3 use my attached .bin.
Any updated information, kindly let me know.
best Regards,
Kerry
Hi @kerryzhou ,
I connected J27 to 0.But I am not able to see VID and PID In NXP-MCU Boot utility.Can we flash the bin using any other method?
Hi @jnj ,
1. serial download mode
When you connected J27 to 0., do you power off and power on the board again?
Or you must do the reset.
If you even can't find the VID, PID, that's strange, seems your chip have issues. As the serial download mode must can be entered if the chip is normal. Please power off and power on, and open the MCUbootutility tool again, whether any improve or not.
2. about downloading.
You can use the JLINK Jflash to download it, the chip you can select the RT1052, as this chip is in default using the hyperflash, other RT1060 is using the QSPI flash driver, it is another story.
Best Regards,
kerry
Hi @kerryzhou ,
I tried flashing bootstrap and bootloader multiple times(Logs of flashing are quite fine).But it is not working.USB is not getting detected in Windows PC.Any memory mapping should be taken care to update ?