1170 SD/MMC manufacture mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1170 SD/MMC manufacture mode

Jump to solution
1,393 Views
MarcoBelli1
Contributor II

I have a doubt regarding SD/MMC manufacture mode described in the 1170 documentation.

According chapter 10.11 SD/MMC manufacture mode, "the boot goes to the SD/MMC manufacture mode before the serial download mode", but according 10.6.6.1 Expansion device eFUSE configuration and Table 26-4. MMC/eMMC boot fusemap SDMMC_MFG_MODE_DISABLE fuse is available only for SD or MMC/eMMC boot mode.

  1. When we set boot mode to internal (boot mode 10) with FlexSPI (bootcfg[7-4] 0000) is "SD/MMC manufacture mode" enabled or not?
  2. In case it's enabled can it be disabled by SDMMC_MFG_MODE_DISABLE fuse?
  3. In case it's enabled do we need to configure some other fuses to configure SD or MMC?
  4. can you link to some documentation about SD/MMC manufacture mode?

 

0 Kudos
Reply
1 Solution
1,363 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Marco,

1. Enable or disable depends on fuse setting not on boot mode. Entering manufacture mode will indeed depend that other boot modes failed.

2. Yes.

3. You mean to use SD/MMC in application or you would like to boot from these? Maybe you can provide more background about what you are trying to implement.

4. Unfortunately, there is no more documentation related to this mode.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

View solution in original post

0 Kudos
Reply
2 Replies
1,364 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Marco,

1. Enable or disable depends on fuse setting not on boot mode. Entering manufacture mode will indeed depend that other boot modes failed.

2. Yes.

3. You mean to use SD/MMC in application or you would like to boot from these? Maybe you can provide more background about what you are trying to implement.

4. Unfortunately, there is no more documentation related to this mode.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply
1,356 Views
MarcoBelli1
Contributor II

I was just trying to understand what "SD/MMC manufacture mode" is about

0 Kudos
Reply