Hello folks !
It seems that RT1170 'EVKB' debug firmware has not MSD. (D&D flash writer)
Is it available somewhere? Maybe I have to 'MAKE' it myself?
I'm VERY confused because NXP's support site still has old 'EVK' information and
hasn't been updated with the new 'EVKB' information.
I'm not saying that old information should be deleted,
but I would like it to be isolated so that people can understand it.
Thank you.
解決済! 解決策の投稿を見る。
This is a report.
We were able to build DAPLINK firmware that allows drag & drop Flash updates.
I was able to do it by adding an entry to the yaml script.
This makes updating in the field (customer site) easier.
We will now move on to designing and manufacturing the hardware.
thank you.
This is a report.
We were able to build DAPLINK firmware that allows drag & drop Flash updates.
I was able to do it by adding an entry to the yaml script.
This makes updating in the field (customer site) easier.
We will now move on to designing and manufacturing the hardware.
thank you.
Mr. Pavel, thank you for your reply.
Judging from the content of the reply, I understand that it does not exist.
I understand that D&D writing cannot be performed with a general-purpose probe
(and probe on board EVKB too)
because it must be generated in combination with a target.
Looks like I'll have to make it myself after all.
Thank you very much again.
Hello, my name is Pavel, and I will be supporting your case, just to get clear, is about the firmware for the debugger probe? if yes, the EVK and the EVKB indeed that different debugger probe, the EVKB has the LPC55s69 McuLink, and the other LPC43 and use LPCScrypt.
To update just need to download the next software.
LinkServer for Microcontrollers | NXP Semiconductors
Use the file depend on the LPC on the board.
Best regards,
Pavel