How to meet the Setup Time and Hold Time of SDRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to meet the Setup Time and Hold Time of SDRAM?

1,118 Views
健鸿凌
Contributor I

01. How to meet the  Setup Time and  Hold Time of SDRAM?
11.png

02. Just follow the means of routing all signals at the same length (±50 mils)?

00.png

03. How to understand the Symbol of   TDVO and  TDHO?

22.png

0 Kudos
Reply
1 Reply

1,047 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

 

  Usually setup and hold time parameters concern inputs,

for outputs delays are used.

 

Looking at the figure 14 above:

 

Setup time is period of SEMC clock / 2 - TDVO;

Hold time is period of SEMC clock / 2 + TDHO.

 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!