How to add program protection function to RT1060 and RT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add program protection function to RT1060 and RT1064

1,551件の閲覧回数
lw3
Contributor I

How to add program protection function to RT1060 and RT1064

Prohibit reading programs through SWD or serial or USB methods

Can encryption function be enabled

Can the flash run normally when switched to another MCU

How to Prevent Copying Flash and Replacing with Other RT1060 MCUs from Running Properly

0 件の賞賛
返信
8 返答(返信)

1,526件の閲覧回数
lw3
Contributor I

After adding read protection to the jlink swd interface

Can we use the swd port of jlink to download new programs again in the future

0 件の賞賛
返信

1,519件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

Yes, please refer to AN12419.

 

Regards,

0 件の賞賛
返信

1,492件の閲覧回数
lw3
Contributor I
Can you give me the download connection for AN12419
0 件の賞賛
返信

1,483件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,432件の閲覧回数
lw3
Contributor I
I'll study how to use it
0 件の賞賛
返信

1,432件の閲覧回数
lw3
Contributor I
Thank you
0 件の賞賛
返信

1,536件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

To prevent unauthorized read from SWD/JTAG, you should enable SJTAG.

To prevent copy code, you should use BEE and encrypt the code in flash.

 

Regards,

Jing

0 件の賞賛
返信