How to Interface OV7620 camera with IMXRT1021

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Interface OV7620 camera with IMXRT1021

908 次查看
jtro
Contributor III

Hi,

I would like to interface OV7620 camera with IMXRT1020-EVK board. I'd seen user manual section 44.5.8 Camera Interface but couldn't found required information also sample code and interface diagram is not available.

Checked Pin mux but no peripheral available to interface camera.

Any application note and sample source code?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

847 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jtro 9 ,

   RT1021 doesn't have the CSI module, then you need to use the FLEXIO to simulate the camera IF, more details you can check the MIMXRT1020 reference manual, 44.5.8 Camera Interface, then you need to use the related flexIO pins.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复