How to Interface OV7620 camera with IMXRT1021

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Interface OV7620 camera with IMXRT1021

788件の閲覧回数
jtro
Contributor III

Hi,

I would like to interface OV7620 camera with IMXRT1020-EVK board. I'd seen user manual section 44.5.8 Camera Interface but couldn't found required information also sample code and interface diagram is not available.

Checked Pin mux but no peripheral available to interface camera.

Any application note and sample source code?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

727件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jtro 9 ,

   RT1021 doesn't have the CSI module, then you need to use the FLEXIO to simulate the camera IF, more details you can check the MIMXRT1020 reference manual, 44.5.8 Camera Interface, then you need to use the related flexIO pins.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信