Hi,
Regarding HW probe for HiFi 4 DSP of i.MxRT685, let me ask.
According to below site, NXP recommend users to use JLINK for HiFi 4 DSP as shown below.
Can you comment if users can use i-Jet instead of JLINK?
You will need to download the necessary J-Link drivers in order to debug the HiFi4 DSP. Follow the next tutorial to see how to download and install this software.
Regards,
Koichi
Hi Kerry,
Thank you for your comment.
I got it.
Regards,
Koichi
Hi @KoichiM
If question is solved, please help to mark the correct answer, just to close this case, thanks.
Any new question, welcome to create the new case.
Best Regards,
Kerry
Hi @KoichiM ,
As I know, the RT685 need to use with the xtensa xplorer IDE, and that need to use with the JLINK, and it will call the related topology.xml, this is using the JLINK.
So, make testing easliy, please refer to the SDK get start to use the JLINK.
BTW, if you are using the MIMXRT685-EVK board, it has the on board JLINK debugger, you don't need to use the external debugger.
Wish it helps you!
Best Regards,
kerry