Further serious bugs in LPSPI driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Further serious bugs in LPSPI driver

1,418 次查看
davenadler
Senior Contributor I

Trying to use LPSPI to interface to a Superior Sensors ND120 shows further serious bugs in the FSL library LPSPI driver.
My fsl_lpspi.h has FSL_LPSPI_DRIVER_VERSION (MAKE_VERSION(2, 4, 0)),
but I verified there's no relevant fix in FSL_LPSPI_DRIVER_VERSION (MAKE_VERSION(2, 6, 6))
Incorrect delays are generated before, during, and after transfer shown by the logic analyzer for the code below:

 

// ND120 has *REALLY SLOW* SPI. Two big nuisances:
// - 6uS clock cycle is 166.666kHz clock (48uSec for 8-bit byte)
// - inter-byte delay of 52uSec is needed for minimum byte cycle time 100uSec
// - 100uSec delay required from CS assertion to first clock
// - 20uSec delay required after last clock til de-asserting CS
// LPSPI:
// - can do delay between 8-bit 'frames' with 'continuous CS' but leaves CS asserted at end of operation?
// - DMA sequencer can do all the above, but perhaps FSL API cannot.
static const lpspi_master_config_t ND120_LPSPI_MasterConfig =
{
	.baudRate = 166666U,					/*!< Baud Rate for LPSPI. 6uS cycle = 166,666Hz */
	.bitsPerFrame = 8, 						/*!< Bits per frame, minimum 8, maximum 4096 */
	// Clock SPI mode '01' (CPOL = 0, CPHA = 1)
	.cpol = kLPSPI_ClockPolarityActiveHigh,	/*!< Clock polarity. */
	.cpha = kLPSPI_ClockPhaseSecondEdge,   	/*!< Clock phase. */
	.direction = kLPSPI_MsbFirst,			/*!< MSB or LSB data shift direction. */
	.pcsToSckDelayInNanoSec = 100000U,		/*!< PCS to SCK delay time in nanoseconds. Spec: 100us */
	.lastSckToPcsDelayInNanoSec = 20000U, 	/*!< Last SCK to PCS delay time in nanoseconds. Spec: 20us */
	// delay is between *FRAMES*
	.betweenTransferDelayInNanoSec = 52000U,/*!< Delay time after SCK in nanoseconds = (100us-8*6us) = 52us. */
	.whichPcs = kLPSPI_Pcs0,                /*!< Desired Peripheral Chip Select (PCS) - over-ridden in transfer API */
	.pcsActiveHighOrLow = kLPSPI_PcsActiveLow,
	.pinCfg = kLPSPI_SdiInSdoOut,			/*!< Set which pins are used for input and output data
											     during single bit transfers, in case some moron wired them backwards.*/
	.dataOutConfig = kLpspiDataOutTristate, /*!< Is output data is tri-stated between accesses (LPSPI_PCS is negated)? */
	/*guess*/.enableInputDelay = false 		/*true caused infinite loop!!*/, /*!< Enable master to sample the input data on a delayed SCK.
 	 	 	 	 	 	 	 	 	 	 *  This can help improve slave setup time. Refer to device data sheet for specific time length. */
};
// FSL LPSPI_MasterInit is buggy: uses inadequate prescale value to support required delays
LPSPI_MasterInit(LPSPI4, &ND120_LPSPI_MasterConfig, BOARD_BOOTCLOCKRUN_LPSPI_CLK_ROOT); // enables clock and LPSI module
// Demonstrate incorrect output on logic analyzer (all delays wrong)
GPIO_PinWrite(BOARD_INITPINS_ND120_RESET_GPIO, BOARD_INITPINS_ND120_RESET_PIN, 0);
vTaskDelay(pdMS_TO_TICKS(1));// 15usec required
GPIO_PinWrite(BOARD_INITPINS_ND120_RESET_GPIO, BOARD_INITPINS_ND120_RESET_PIN, 1);
vTaskDelay(pdMS_TO_TICKS(80));// first response settling time after RESET
uint8_t exampleTx[3] = {1,2,3};
uint8_t exampleRx[3] = {0};
const lpspi_transfer_t transfer =
{
	.txData = (uint8_t*)exampleTx, /*!< Send buffer. */
	.rxData = (uint8_t*)exampleRx, /*!< Receive buffer. */
	.dataSize = (size_t)3,         /*!< Transfer bytes. */
	.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous,
};
lpspi_transfer_t t1 = transfer; // **bleep**ed-up API requires non-const transfer structure
status_t s1 = LPSPI_MasterTransferBlocking(LPSPI4, &t1);
assert(s1 == kStatus_Success); (void)s1;

 

Note the incorrect delays in the scope image:
All delays are wrong...All delays are wrong...

Analyzing the FSL code shows the following bugs:

1) Delays are set to somewhat random values rather than correct results after the FSL code determines it cannot set correct values! In all cases this should generate an error, ideally an assert failure for debug builds. It is unacceptable to silently do the wrong thing!

2) The maximum required delay must be used to establish the minimum prescale value which allows all delay values to fit in the available 8-bit fields. For the example above this prescale value is 5, but the code incorrectly sets 1!

3) In all cases, datasheets (as the one linked above) show minimum required delays and maximum allowable clock speeds. The FSL code goes through a convoluted iteration trying to find the closest value! The correct delay values are the smallest delay above or equal to the specified delays. The correct clock divisor is the fastest possible rate slower than or equal to than the requested clock. These values can be easily calculated with no iteration required!

4) The FSL code uses a lookup table to get 1 raised to a power of 2, rather than a shift operator!

5) Using "continuous" mode here, the bytes are sent in the correct order, unlike previous examples I posted. The driver completely ignores the kLPSPI_MasterByteSwap flag and sends bytes in correct order regardless of setting!

6) In LPSPI_MasterInit, the delay times are set in CCR after enabling the module. In addition, the LPSPI_MasterSetDelayTimes routine has no assertion to verify it is only called when the module is disabled.

7) LPSPI_MasterInit does not reliably re-initialize an LPSPI module. In my case:
- I initialized for sensor A, and IO proceeded correctly.
- I initialized for sensor B, corrected wrong values for CCR and prescale, and IO proceeded correctly.
- I re-initialized for sensor A, and IO proceeded at wrong speed.
Apparently LPSPI_MasterInit does not actually initialize everything...

Has anyone in the community written a working LPSPI driver?
The FSL driver is quite unusable with all these bugs...

Thanks,
Best Regards, Dave

PS: For the example above, here are the correct LPSPI register settings:

 

// LPSI delays are computed using LPSI_clockHz = (LPSPI_CLK_ROOT/(1<<clockPrescalerExponent)),
// and *NOT* the Clock Control Register CCR divisor used to generate SPI clock signal.
// The SPI clock divisor and delay fields are only 8 bits, so:
// - 255*LPSI_clockHz_Period must be > max desired delay (100uSec here) -> minimum prescale of 5
// - clock signal divisor must also fit -> minimum prescale of 1
// We're using the slowest possible LPSPI_CLK_ROOT of 66MHz (period ~15nSec)
const uint32_t clockPrescalerExponent = 5; // set in transfer control word in FIFO (TCR), not Clock Control Register CCR
const uint32_t LPSI_clockHz = BOARD_BOOTCLOCKRUN_LPSPI_CLK_ROOT / (1<<clockPrescalerExponent); // 66MHz/32 = 2,062,500Hz
const uint32_t LPSI_clockPeriodNsec = 1000000000U/LPSI_clockHz; // 484
const uint32_t clockDivisor = LPSI_clockHz / 166666U; // 166,666Hz for 6uS cycle
const uint32_t LPSI4_CCR_ND120 =
		(clockDivisor-1)                    << LPSPI_CCR_SCKDIV_SHIFT |
		(( 52000/LPSI_clockPeriodNsec)+1)   << LPSPI_CCR_DBT_SHIFT    |  // delay between continuous frames = 100uSec - 8*6uSec clock periods
		((100000/LPSI_clockPeriodNsec)+1)   << LPSPI_CCR_PCSSCK_SHIFT |  // delay from CS to first clock
		(( 20000/LPSI_clockPeriodNsec)+1)   << LPSPI_CCR_SCKPCS_SHIFT ;  // delay from last clock to de-asserting CS
LPSPI4->CCR = LPSI4_CCR_ND120;
LPSPI4->TCR |= clockPrescalerExponent<<LPSPI_TCR_PRESCALE_SHIFT;
​

 

 

标记 (3)
4 回复数

909 次查看
splatspeed1
Contributor I

hi David just started with the EVM seeing similar issues we were going to track this down and see if we can fix the issue, which example did you start with? @davenadler 

0 项奖励
回复

1,129 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @davenadler,

Thank you for such an in-depth insight about our LPSPI drivers.

I have reported your findings from this post (along with the previous one you share) with the internal applications team for them to deliberate and fix on a future release of our SDKs. It seems like this issue is well ingrained into the driver of several i.MX RT devices, so if they conclude that a workaround is necessary, the change might still take some time to be fully implemented in all of our SDKs.

Once again, we appreciate the great effort from your side to take the time to investigate this issue and report it.

BR,
Edwin.

0 项奖励
回复

1,305 次查看
davenadler
Senior Contributor I

1,338 次查看
davenadler
Senior Contributor I

Hoping someone at NXP can respond here:

  • Have you used the provided example code to replicate and verify the bugs listed?
  • Does NXP have any plans to fix this, or is the FSL driver library no longer supported and we should not use iMX.RT parts for new projects?

Thanks,
Best Regards, Dave