FLEX IO in low power run mode (RT1015)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEX IO in low power run mode (RT1015)

Jump to solution
2,063 Views
kensu
Contributor V

Hi,

I am testing UART Flex IO in low power run mode in 1015RT.

I use the SDK sample and combine UART Flex IO sample.

Please see my attachment.

My code hang up when UART_FlexIO_Init, 

pastedImage_2.png

As I know, Flex IO can use in low power mode.

pastedImage_1.png

What is the correct way to use UART_FlexIO in low power run mode?

Any limitation?

Or any suggestion?

Thanks

Ken

Labels (1)
1 Solution
1,908 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

  A lot of talks with an internal side, it turns out the document error.

  1. PLLs for FlexIO is powered down under low power run mode

    Please check the RT1050RM, RT1015RM still didn't update it, AN12345 is also incorrect, already report it.

pastedImage_1.png

2. pll3_sw_clk_sel =1 option should not be used, That bit is intended for NXP internal test and uses an input clock on a pin instead of the internal PLL bypass clock. So it is a different kind of bypass than what is implied in the description.

This part will be removed from the document.

3. The FlexIO module allows for functional clock to run in low power modes (and really this statement is a carry over from Kinetis), but the SOC integration on RT10xx parts does not.

I also suggest our related department to add peripheral states to the low power mode definitions table.

In conclusion, FlexIO module can't be used under low power run mode.

Sorry for the inconvenience we bring you.

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

9 Replies
1,908 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su ,

   Please check the RT1015 power consumption application note at first:

https://www.nxp.com/docs/en/application-note/AN12345.pdf 

 pastedImage_2.png

Then check your code, your code FLEXIO is using the usbPLLclk, but from the application note, you can find in the low power run mode, all the PLLS are powered down, that's why you hang up there.

So, you need to check other clock source for flexio which still works under low power run mode.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,908 Views
kensu
Contributor V

Hi Kerry

Thanks for your remind,

Frankly speaking, I don't know very well about the CLK setting,

Could you let me known how to use FlexIO in low power run mode?

pastedImage_1.png

pastedImage_2.png

I think it need to change  FLEXIO1_CLK_SEL to OSC so that I can use FlexIO UART in low power run. 

Is it possible? 

Regards

Ken

0 Kudos
Reply
1,908 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

  Thanks for your updated information.

  Today, I do the testing, bypass the PLL3, and select the FlexIO1 clock source as PLL2_SW_CLK, PLL2_SW_CLK bypass the PLL3, and from the 24Mhz directly, but it seems still have an issue when I enable the FlexIO1 clock gate and access the FLEXIO1 register.

pastedImage_1.png

pastedImage_2.png

Anyway, I will help you to check it internally.

If I get valuable information, I will also let you know.

Please keep the patient, thanks.

Best Regards,

Kerry

0 Kudos
Reply
1,908 Views
kensu
Contributor V

Hi Kerry

Thanks a lot for your support.

I will wait.

Best Regards

Ken

0 Kudos
Reply
1,908 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

   Get the internal response: Unfortunately, the FlexIO cannot be used in low power run mode.

   But more details, I am still checking more deep level.

   Please keep the patient!

Best Regards.

Kerry

0 Kudos
Reply
1,908 Views
kensu
Contributor V

Hi Kerry

OK, I understood.

I will wait your information.

Thanks.

Best Regards

Ken

0 Kudos
Reply
1,909 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

  A lot of talks with an internal side, it turns out the document error.

  1. PLLs for FlexIO is powered down under low power run mode

    Please check the RT1050RM, RT1015RM still didn't update it, AN12345 is also incorrect, already report it.

pastedImage_1.png

2. pll3_sw_clk_sel =1 option should not be used, That bit is intended for NXP internal test and uses an input clock on a pin instead of the internal PLL bypass clock. So it is a different kind of bypass than what is implied in the description.

This part will be removed from the document.

3. The FlexIO module allows for functional clock to run in low power modes (and really this statement is a carry over from Kinetis), but the SOC integration on RT10xx parts does not.

I also suggest our related department to add peripheral states to the low power mode definitions table.

In conclusion, FlexIO module can't be used under low power run mode.

Sorry for the inconvenience we bring you.

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,908 Views
kensu
Contributor V

Hi Kerry

It's OK.

Very appreciate for your detail information.

Regards

Ken

0 Kudos
Reply
1,908 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su

   You are always welcome!

   If your question is solved, please help me to mark the correct answer, just to close this case, thanks.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------