Executing a task (code) only in one specific core in MXRT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Executing a task (code) only in one specific core in MXRT1170

ソリューションへジャンプ
648件の閲覧回数
Shehan_Janidu
Contributor III

I am new to nxp semiconductors and I need to use MXRT1170 CHIP. I want select specifically one core from this dual core processor and execute a code on it. Can anyone guide me with references of reference manual to do the necessary configurations to the firmware. I am using keil uvision5 as IDE. 

Can u show me a sample code for it

0 件の賞賛
返信
1 解決策
620件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Shehan_Janidu,

I recommend you to look into our multicore example codes on the SDK, since they illustrate the usage of a dual core application with the RT1170, and are easy to modify according to your needs. For more detailed information about how these example codes (or any dual core application) work, please look into the following application note: https://www.nxp.com/docs/en/application-note/AN13264.pdf

BR,
Edwin.

元の投稿で解決策を見る

1 返信
621件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Shehan_Janidu,

I recommend you to look into our multicore example codes on the SDK, since they illustrate the usage of a dual core application with the RT1170, and are easy to modify according to your needs. For more detailed information about how these example codes (or any dual core application) work, please look into the following application note: https://www.nxp.com/docs/en/application-note/AN13264.pdf

BR,
Edwin.