I am new to nxp semiconductors and I need to use MXRT1170 CHIP. I want select specifically one core from this dual core processor and execute a code on it. Can anyone guide me with references of reference manual to do the necessary configurations to the firmware. I am using keil uvision5 as IDE.
Can u show me a sample code for it
已解决! 转到解答。
Hi @Shehan_Janidu,
I recommend you to look into our multicore example codes on the SDK, since they illustrate the usage of a dual core application with the RT1170, and are easy to modify according to your needs. For more detailed information about how these example codes (or any dual core application) work, please look into the following application note: https://www.nxp.com/docs/en/application-note/AN13264.pdf
BR,
Edwin.
Hi @Shehan_Janidu,
I recommend you to look into our multicore example codes on the SDK, since they illustrate the usage of a dual core application with the RT1170, and are easy to modify according to your needs. For more detailed information about how these example codes (or any dual core application) work, please look into the following application note: https://www.nxp.com/docs/en/application-note/AN13264.pdf
BR,
Edwin.