I am using the MIMXRT595-EVK development board, which has an i.MX-RT500 chip with a 2-lane MIPI DSI output.
Currently, the requirement is to drive two 1-lane displays.
The content to be displayed should be completely synchronized and identical on both screens.
Does the RT500 chip support this setup?
解決済! 解決策の投稿を見る。
Hi @mintisan
The i.MX RT500 chip does support MIPI DSI output, but it's important to note that it only has a single 2-lane MIPI DSI interface. This means that while it can drive a single 2-lane display, it cannot directly drive two 1-lane displays simultaneously.
However, you may be able to achieve your goal by using a MIPI DSI splitter or bridge chip. This would take the 2-lane output from the i.MX RT500 and split it into two 1-lane outputs. Please note that this is an assumption and the actual feasibility would depend on the specific requirements of your project and the capabilities of the splitter or bridge chip you choose.
For more information on the i.MX RT500's MIPI DSI capabilities, you can refer to the i.MX RT500 MIPI DSI Interface article on the NXP Community site.
For code examples and further technical details, you can also refer to the i.MX RT Series Software and Development Tools article.
Hi @mintisan
The i.MX RT500 chip does support MIPI DSI output, but it's important to note that it only has a single 2-lane MIPI DSI interface. This means that while it can drive a single 2-lane display, it cannot directly drive two 1-lane displays simultaneously.
However, you may be able to achieve your goal by using a MIPI DSI splitter or bridge chip. This would take the 2-lane output from the i.MX RT500 and split it into two 1-lane outputs. Please note that this is an assumption and the actual feasibility would depend on the specific requirements of your project and the capabilities of the splitter or bridge chip you choose.
For more information on the i.MX RT500's MIPI DSI capabilities, you can refer to the i.MX RT500 MIPI DSI Interface article on the NXP Community site.
For code examples and further technical details, you can also refer to the i.MX RT Series Software and Development Tools article.
Thanks for your reply.
But I can't access https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/i-MX-RT500-MIPI-DSI-Interface/ta-p/1105464...
How can I access URL above? Thanks...
```
Click your browser's Back button to continue.
```
Hi @mintisan
Giraffe is an AI robot. We don't know who manipulate it. So you know the link it gave is nonsense.
But it's true RT500 can't support your idea. You can refer to AN13573 and AN12940.
Regards,
Jing