Configure Custom SRAM Partition in IMXRT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configure Custom SRAM Partition in IMXRT1064

845 次查看
prashanthkk
Contributor II

Dear All,

 

We are using iMXRT1064 EVM board for our testing in which we are going to partition its internal SRAM from 1MB.

Below is our requirement.

SRAM_DTC:     256 KB 
SRAM_OC:       768 KB

For this we changed system GPR registers to below one,

In board.c file,

/* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(6, 0x20000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB);

/* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(7, 0x20200000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512KB);

There is no region selection for 768KB in 'ARM_MPU_RASR' register settings.

 

Also we have done below register settings in startup code.

"LDR R0, =0x400ac044\n"//Address of register IOMUXC_GPR_GPR17
"LDR R1, =0xAAAAAAAA\n"
"STR R1,[R0]\n"

"LDR R0,=0x400ac040\n"//Address of register IOMUXC_GPR_GPR16
"LDR R1,[R0]\n"
"ORR R1,R1,#6\n"//The 4 corresponds to setting the FLEXRAM_BANK_CFG_SEL bit in register IOMUXC_GPR_GPR16
"STR R1,[R0]\n"

"LDR R0,=0x400ac040\n"//Address of register IOMUXC_GPR_GPR16
"LDR R1,[R0]\n"
"AND R1,R1,#0xfffffffe\n"//Disabling SRAM_ITC in register IOMUXC_GPR_GPR16
"STR R1,[R0]\n"

"LDR R0, =0x400ac038\n"//Address of register IOMUXC_GPR_GPR14
"LDR R1, =0x900000\n"//New size configuration for the IOMUXC_GPR_GPR14 register
"STR R1,[R0]\n"

 

But still above configuration is not working for us.

After board flashing, its showing as 'Break at address "0xdeadbeee" with no debug information available, or outside of program code.'

 

Kindly please help us to proceed further.

 

Thanks & Regards.

Prashanth Kumar K

标签 (1)
0 项奖励
回复
1 回复

822 次查看
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @prashanthkk 

You can check this doc https://www.nxp.com/docs/en/application-note/AN12077.pdf, may be can help you with this problem.

 

with 'Break at address "0xdeadbeee" with no debug information available, or outside of program code.', Did this occurred when you run a example program too?

Have a good day

Bests Regards

 

Carlos

 

0 项奖励
回复