The original sd_jpeg code is written for a 480×272 LCD panel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The original sd_jpeg code is written for a 480×272 LCD panel

Jump to solution
879 Views
KHSALEH
Contributor I

Please I need a copy of the original sd_jpeg.c for a 480x272 LCD referenced in AN12302.

I'm having difficulty configuring the RK043FN02H-CT TFT display, the sd_jpeg.c may provide some help.

Best regards

0 Kudos
Reply
1 Solution
853 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
Please click the SELECT ALL option, then download the complete SDK library.
After that, you can find the sd_jpeg demo as the below figure shows.

jeremyzhou_0-1644992297413.png

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
3 Replies
865 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the sd_jpeg demo in the SDK library for the MIMXRT1050.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
859 Views
KHSALEH
Contributor I

Thank you for your reply. Please note I've tried the link provided, but the downloaded SDK does not contain sd_jpeg demo. It appears I'm lost in filtering and selecting the sought for SDK. Please advise a more direct link to the required file.Untitled.jpg

0 Kudos
Reply
854 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
Please click the SELECT ALL option, then download the complete SDK library.
After that, you can find the sd_jpeg demo as the below figure shows.

jeremyzhou_0-1644992297413.png

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply