Hello. I have compilation error from SDK_2.9.1_MIMXRT1021xxxxx. Project: evkmimxrt1020_lwip_udpecho_freertos (I tried all lwip examples - the result is always the same)
../source/lwip_udpecho_freertos.c:21:10: fatal error: ethernetif.h: No such file or directory
21 | #include "ethernetif.h"
| ^~~~~~~~~~~~~~
compilation terminated.
There is no such file in example. I am using latest SDK (2.9.1) and latest MCUXpresso IDE v11.3.0.5222.
解決済! 解決策の投稿を見る。
Deleting older SDK from "installed SDKs" solved the problem. Dont understand how can it influence, but problem is solved.
Hi nda,
Thanks for your updated information.
I checked your SDK2.9.1 for MIMXRT1020, in fact it is used for azuarertos, not the freertos.
So, if you run the freertos code, I suggest you download the SDK2.9.0, and delete the 2.9.1 in installed SDKs, add the SDK2.9.0,freertos version:
Wish it helps you!
Best Regards,
Kerry
Deleting older SDK from "installed SDKs" solved the problem. Dont understand how can it influence, but problem is solved.
There are also problems with USB examples. Соmpiling of evkmimxrt1020_dev_cdc_vcom_freertos:
In file included from ../usb/device/class/cdc/usb_device_cdc_acm.c:21:
../usb/device/class/cdc/usb_device_cdc_acm.h:130:5: error: unknown type name 'usb_osa_mutex_handle'
130 | usb_osa_mutex_handle mutex; /*!< The mutex of the pipe. */
| ^~~~~~~~~~~~~~~~~~~~
Only simple base examples have no errors :(((((