Chipset comination of RT1052 + PN7150 for payment system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chipset comination of RT1052 + PN7150 for payment system

ソリューションへジャンプ
1,363件の閲覧回数
andy_kim
Contributor IV

Hello,

We've used RT1052 on our device.

and We're planning to add PN7150 for contactless payment system on it.

 

I wonder if that chipset combination is no problem for working as payment system.

Or  Shoule we use KL81 MCU + PN7150 for contactless payment system?

 

Thank you,

Andy

0 件の賞賛
返信
1 解決策
1,349件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,356件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Shoule we use KL81 MCU + PN7150 for contactless payment system?
-- Benefit from the rich security features, I consider the KL81 is better choice than the RT1052.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,351件の閲覧回数
andy_kim
Contributor IV

Hi, Jeremyzhou

Thanks for your prompt reply and comments.

Actually, we just use NFC technology for contactless payment.

As far as I know, K81/KL81 is a solution for POS teminal which supports contact card, contactless card and magstripe card for payment.

Do you think RT1050 have a security risk when using it for contactless payment solution?

 

Thank you

Andy

0 件の賞賛
返信
1,350件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Andy,
Thanks for your reply.
1) Do you think RT1050 has a security risk when using it for a contactless payment solution?
-- Yes.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,329件の閲覧回数
andy_kim
Contributor IV

Hi, Jeremyzhou,

 

Thanks for your reply.

 

Let me close this case

 

Thank you,

Andy

0 件の賞賛
返信