Can I use ST-Link V2 to program the smart voice board(SLN-SVUI-IOT)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use ST-Link V2 to program the smart voice board(SLN-SVUI-IOT)?

1,023件の閲覧回数
AndryckSant
Contributor II

Hello community,

 

I am trying to flash the micropython firmware on NXP's smart voice board(SLN-SVUI-IOT). It is a board project based on another board, the MiMXRT1060.

 

I realized that in the Smart Voice's schematics, it does not have an onboard debugger. I was wondering if I can use an original ST-Link V2 to program the smart voice board and flash the micropython firmware. I also noted that the "STM32" port of the ST-Link has a 20 pin JTAG port. The smart voice board has a 10 pin JTAG port. I can use some kind of adapter on it?

 

Or I was also wondering if I could use a specific hardware with the daplink firmware to program the board. Here is the link of the hardware mentioned: https://pt.aliexpress.com/item/1005005634441693.html?spm=a2g0o.productlist.main.1.78d4205f4bniF9&alg...

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,005件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can use the debugger on MXRT.

Regards

0 件の賞賛
返信

1,000件の閲覧回数
AndryckSant
Contributor II

I think this board does not have a debugger.

 

I'm with a Smart Voice board(SLN-SVUI-IOT)

 

please, take a look at its schematics.

 

best regards, 

Andryck Santiago

0 件の賞賛
返信