We have prototypes of our RT1062 design with octal hyperflash and octal hyperram (2 die in one package) and I am working on software. The two devices use FLEXSPI A and B data[3:0], and FLEXSPI_A_SS0_B, FLEXSPI_A_SS1_B, as in fig 27-3 of the RT1060 reference manual. We would like to boot & run XIP on the hyperflash, and ideally access the hyperram via AHB for general data storage/buffer.
I have code running XIP from the hyperflash, but don't quite have the hyperram running yet. IP write/read does not give the same data, and AHB accesses cause a hardfault / bus error. I note these two posts
https://community.nxp.com/t5/i-MX-RT/Question-about-Using-HyperRam-and-HyperFlash/m-p/971681
and would like to get some confirmation that what I am trying to do is possible before I spend too much time trying to get it to work. I cannot find any information in the Reference Manual or Errata that suggests running XIP precludes the use of a second device on the FLEXSPI in octal mode, with AHB access.
Can anyone authoritatively confirm that operation of two octal hyperbus devices on the 1062 FLEXSPI is possible or not, with XIP for one device, and AHB access on the other? (If not possible, perhaps this should be noted in the Reference Manual or Errata?)
Cheers,
Mark
解決済! 解決策の投稿を見る。
In principle, HyperFlash and HyperRAM could be connected to one FlexSPI instance if these two memories have the same electrical properties. but in this case, XIP performance may be bad as they share the same data port.
FlexSPI IP can handle this scenario: with XIP for one device, and AHB access on the other
Hi berban,
No, I gave up. I played with the flexspi LUT command sequences, and got the hyperflash to program. But I didn't get as far as running code.
Cheers,
Mark
Thank you. I will persist with my exploration of FLEXSPI config. We expect to use the second device (RAM) rarely, and can place time critical code in ITC.
In principle, HyperFlash and HyperRAM could be connected to one FlexSPI instance if these two memories have the same electrical properties. but in this case, XIP performance may be bad as they share the same data port.
FlexSPI IP can handle this scenario: with XIP for one device, and AHB access on the other