7 INCH DISPLAY WITH IMXRT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

7 INCH DISPLAY WITH IMXRT1176

1,385件の閲覧回数
saket
Contributor I

I am trying to interface 7 inch display(RK070CU05H) with imxrt1176, what changes should I make in sdk to make it work ? I have attached datasheet of display.

0 件の賞賛
返信
5 返答(返信)

775件の閲覧回数
sakethh
Contributor I

Hi @EdwinHz ,

I tried Using GUI GUIDER but didn't got the result, can you please provide the procedure to walk through the gui guider for setting the 7 inch display(RK070CU05H) 1024*600 resolution display.

 

0 件の賞賛
返信

1,366件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @saket,

All of the necessary changes should be contained within the 'display_support.c' and 'display_support.h' files, which are under the 'board' folder of our example projects.

From the display_support.h file, you should make sure to adjust the panel width and height and select the appropriate pixel format. The panel controller can stay the same.

From the display_support.c file, you should make sure to adjust the synchronization signals according to your display's specifications (HSW, HFP, VSW, etc.), and ensure the MIPI and the LCD controller and the PHY clocks are properly configured. These clocks are initialized on the routines BOARD_InitMipiDsiClock of the BOARD_InitLcdifClock() respectively.

For more detailed information about the integration of LCD panels with the RT1170, please look into the following application note: AN12940: Use Case of RT1170 LCD Display System based on MIPI DSI – Application Note (nxp.com).

BR,
Edwin.

 

0 件の賞賛
返信

1,337件の閲覧回数
sakethh
Contributor I

Hi @EdwinHz ,

In the SDK fbdev_freertos display example 3 5inch displays and their driver IC's are also mentioned like fsl_rm68200,fsl_hx8394,fsl_rm68191 along with their .c and .h file . So, if i need to implement 7 inch display , there is no driver IC mentioned in RK070CU05H document. what should id do? and how can we configure  MIPI and the LCD controller and the PHY clocks?

0 件の賞賛
返信

1,318件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @sakethh,

My recommendation would be to use a GUI Guider project with a custom panel of 1024x600 resolution as a base project for your application. This will allow you to customize the graphical interface in a friendly manner, while having a complete project which would only require a few tweaks to make sure it works with your hardware.

BR,
Edwin.

0 件の賞賛
返信

741件の閲覧回数
sakethh
Contributor I

Hi @EdwinHz ,

I tried using GUI Guider but didn't get any output on the 7-inch 1024x600 resolution display. Can you provide a walkthrough of the procedure to make the display work ?

0 件の賞賛
返信